Related Tags
Now, 28 AWG patch cords are finding their way into AV applications, too. With IoT devices like digital signage displays, projectors and phones connecting to networks via PoE cable, AV professionals have been asking: Can smaller-diameter patch cords (such as 28 AWG) be used in PoE applications to save space there as well?
The answer: yes! But there are a few things to keep in mind. Want to learn more about using 28 AWG patch cords in AV applications? Read the blog in its entirety here!
作者简介
格雷格·芬克
现场应用工程师
格雷格·芬克 (Greg Funk) 于 1984 年开始其职业生涯,担任分布式计算机网络分析师。 Greg 在 Belden 工作了二十多年,是 Belden 的数据中心专家之一,也是行业研讨会和活动的知名演讲者。 他担任过多种职务,是一名现场应用工程师,为其所在地区提供网络工程销售支持。