1. Fiber Supports Very High Bandwidth Levels
When it comes to bandwidth, no currently available technology is better than fiber – especially singlemode fiber. Fiber optic cables provide more bandwidth to carry more data than copper cables of the same diameter.
No matter what new fiber-optic technologies make it to market in terms of transceivers or other electronics, the benefits of fiber include the fact that its performance isn’t limited by the cable itself. Instead, it’s limited by the electronic components that make up the system. Upgrade the components and your fiber cabling will be good to go.
Latency decreases with fiber as well, enabling faster download and upload times, as well as faster access to resources. Because of this low loss, fiber can also carry data across longer distances without delays or interruptions.
2. Fiber is Inherently Secure
Fiber cables don’t emit signals; connecting taps to a fiber cable to intercept data transmission is incredibly difficult.
Because the signal traveling through a fiber cable is contained inside the individual fiber strand, it must be accessed from the end of the cable by cutting into it. In most cases, this would take the network down, and everyone would quickly become aware of the issue.
3. Fiber is Intrinsically Safe
Because electricity isn’t involved with transferring data (data is transferred via light instead), the benefits of fiber include the fact that it’s safe to handle.
4. Fiber Withstands Water and Temperature Fluctuations
Fiber optic cable isn’t impacted by temperature changes, bad weather or moisture. For example, if it comes into contact with rainwater, communication goes on as usual. If lightning strikes a fiber cable, the surge of electricity will not be propagated because the fiber cable doesn’t contain any metallic components.
It can withstand harsh environments without any changes in performance, making it ideal for rugged environments like outdoor, long-distance and industrial applications.
5. Fiber is Immune to EMI
Placing lots of electronic cables (which carry electric current) in a dense environment can create crosstalk between cables – which causes performance issues and data-transmission interruption.
Fiber cables, however, don’t produce electromagnetic interference (EMI). They aren’t impacted by EMI, either. You can deploy them right next to industrial equipment without worry.
Would the benefits of fiber mesh well with the requirements of your next project? Contact one of our fiber experts to learn more or visit our fiber system webpage.
作者简介
Nelson Oliver
工程师
尼尔森·奥利弗 (Nelson Oliver) 于 2015 年加入 Belden 担任光纤产品工程师,拥有强大的工程背景。 拥有罗斯霍曼理工学院光学工程理学学士学位。 在目前任职于 Belden 期间,Nelson 专门为企业应用设计和开发可靠的光纤布线解决方案。