3D-Smart-Cityscape-Futuristic-Blueprint

I’d like to give kudos to both gentlemen—the first, for thinking of the resources and expertise of his IT colleagues in the heat of the moment, and the second, for so effectively and dramatically illustrating a concern that is so much in discussion today—the ambivalence and lack of understanding that can exist between OT and IT colleagues.

 

2018-07-11-is-blog-image1

 

A New Era of Cooperation

As industry works – with varying degrees of success – to create a new world of IT/OT convergence and partnership, with the previously distinct lines and silos between the roles and responsibilities of each becoming more blurred, it pays to keep the comments of the Ukrainian operators in mind. If there had been greater teamwork between OT and IT in the plant in the months preceding, might the attack have been avoided or been mitigated in some way?

 

Whether or not that would have been the case, there are, unfortunately, more and more opportunities to ask the question. There has been a sharp increase in cyber attacks against industrial control systems, including a recent one that targeted plant safety instrumentation systems in the oil and gas industry. It’s a disturbing increase in the level of maliciousness to think that human life could be targeted and not just equipment. Another frightening warning sign of possible things to come relates to a recent technical alert sent out by the U.S. Industrial Control Systems Cyber Emergency Response Team (ICS-CERT). CERT warned that a hacked schematic of an 8.8 megawatt turbine belonging to an American power plant was retrieved from a Russian command and control server. Conjecturing what that could mean is a very scary exercise. (On the positive side, being forewarned is the first step towards being forearmed. If you're not yet subscribing to outstanding alerts, advisories, reports and other invaluable resources from ICS-CERT, please consider doing so.)

 

In late 2017, Belden’s Tripwire group once again teamed with SANS Institute on their annual survey of ICS and plant operations engineering professionals to help provide a little insight. Among the disturbing findings: nearly 70% of respondents—insiders all—consider the current threat to their systems to be high or severe/critical. Their biggest single concern, they report, are devices unable to protect themselves being added to the network. A top attack concern is ransomware, which is exploding, with levels nearly doubling year over year. This is the environment that we are in today.

 

2018-07-11-is-blog-image2

 

How to Leverage the Expertise on the Other Side

While we at Tripwire and Belden have many OT clients with fairly sophisticated cybersecurity resources, for the vast majority of organizations, the bulk of cyber security expertise resides in the IT department. After all, they have been doing it far longer than their OT colleagues and have been building expertise and organizational infrastructure over decades. And that’s good news—it means that OT doesn’t need to reinvent the wheel and build a new organization from scratch. Instead, they simply need to bridge the gap between IT and OT to accelerate their ability to ward off escalating threats and continue bolstering their cyber security.

 

IT has plenty to learn from OT as well. OT’s earned expertise in prioritizing uptime and resiliency can no doubt find applications in other areas of the organization, as can their unrelenting focus on safety. Safety, of course, had never before been a driving priority in the IT world, but it’s something that will need to become more pronounced as the silos between IT and OT inevitably crumble.

 

So how can OT and IT pros ease the transition? In a perfect world, the drivers will come from senior management, who create the structure of the organization and codify expectations in formal policy and procedure “bibles” as well as in directions to their staff. But more informally, each of us can work to get to know colleagues on the other side of the “T” and reach out to them for relevant advice, never forgetting that there is a vital human element to the IT/OT convergence as well as a technological one. Maybe ask OT or IT managers to set up joint meetings focusing upon common goals. If appropriate, perhaps even ask for an embedded colleague; for example, an IT cyber security expert on full- or part-time loan to help with OT challenges. All organizations are different of course, but the OT/IT convergence will no doubt be looked back upon as a turning point in industry’s fight for cyber security and further harnessing of technology for business success. Being an early, proactive leader in that regard certainly, in general, seems like a good role to be playing.

 

For a look at some other cyber security trends and business challenges, view our on-demand webinar Challenges and Checklists: Defending Control System Cyber Assets.

 

We at Belden and Tripwire work with a lot of different organizations in varying stages along the IT/OT convergence continuum. We might be able to provide insight to issues you may be having. Call us and we’ll be glad to start a dialog.

作者简介

Robert Landavazo

Tripwire系统工程师

Robert Landavazo 是 Tripwire 的系统工程师,他专注于帮助客户保护他们的工业控制系统。 他拥有电力公用事业领域的背景,最近致力于利用 Tripwire 自己的产品套件实施 NERC 关键基础设施保护 (CIP) 内部合规计划。 在这家公用事业公司任职期间,罗伯特从事运营技术工作,为配电、输电和发电领域的 SCADA 提供支持。 在从事公用事业工作之前,罗伯特曾在公共安全领域工作,负责管理紧急通信基础设施,例如下一代 911、IP 无线电和计算机辅助调度系统。